Produktoplysninger
Produktoversigt
An international best-seller, the Wave Plus has all the essential tools of the original with the addition of replaceable, durable wire cutters. All 18 tools can be opened and locked quickly, conveniently to tackle any task. Many of these tools are outside-accessible, so you can use them when the multi-tool is folded and closed.
- This multi-tool features tools that are accessible while the tool is in its folded or closed position, mimicking the functionality of a pocket knife
- Every feature on this tool can be opened and operated with one hand
- This enables the user to keep the other hand free for situations that require multi-tasking or a free hand
- An improved, high-carbon (HC) form of 420 stainless steel that works well with high production tooling - optimised in Leatherman multi-tools by heat treatment
- Lanyard Ring - This secure ring is for attaching the tool safely and securely to a lanyard
- Often people who work near water or on scaffolding attach their tool to a lanyard on their person to avoid losing the tool if it's dropped
- Open Length: 15.87cm
- Closed Length: 10cm
- Primary Blade Length: 7.37cm
- Weight: 241g
Indhold
Tools: Needlenose Pliers, Regular Pliers, Premium Replaceable Wire Cutters, Premium Replaceable Hard-Wire Cutters, Electrical Crimper, Wire Stripper, 420HC Knife, 420HC Serrated Knife, Saw, Spring-Action Scissors, Ruler (8in / 19cm), Can Opener, Bottle Opener, Wood/Metal File, Diamond-Coated File, Large Bit Driver, Small Bit Driver, Medium Screwdriver
Advarsler
It is illegal to sell this item to anyone under 18 years of age. Orders containing this item will be subject to an age verification process and proof of age will be required upon delivery to residential addresses.
Tekniske specifikationer
-
Leatherman - Wave Plus
-
To Be Advised
Tekniske dokumenter (2)
Lovgivning og miljø
Det land, hvor den sidste væsentlige fremstillingsproces fandt stedOprindelsesland:United States
Det land, hvor den sidste væsentlige fremstillingsproces fandt sted
Certifikater om produktoverholdelse