Introduction

An industrial robot is a programmed mechanical device that performs production-related jobs automatically in industrial environments. In the industrial and automation world, robots use sensors to create a picture of their surroundings. Industrial robots utilise several sensors to achieve reasonable control and operation in industrial automation production processes. The manufacturer can add various sensors to different robots to increase their adaptability, ensuring higher profitability with a lower cost per product by reducing the potential for human fatigue and error. This article discusses, in brief, the top ten necessary industrial robot sensors.

Sensors used in industrial robots

The continuous and rapid introduction of several new sensor technologies plays an essential role in developing more advanced industrial robots. The ten most used sensors in industrial robots are:

  1. Two-dimensional vision sensor

    It is a smart camera that can perform many tasks, including detecting moving objects and finding parts on the conveyor belt. The robot can appropriately adjust its motion based on the received information.

    two-dimensional-vision-sensor
    Figure 1: Two-dimensional vision sensor
  2. Three-dimensional vision sensor

    The 3D vision system can detect the object’s third dimension. It uses two cameras or laser scanners at different angles to perform its function. For example, part picking and placing using 3D vision technology to detect objects and create 3D images. It also analyses and selects the best picking method.

    three-dimensional-vision-sensor
    Figure 2: Three-dimensional vision sensor
  3. Navigation (positioning) sensors

    Navigation or Positioning sensors approximate the robot’s position. The standard positioning sensor is a GPS (Global Positioning System). A robot receiver acquires and processes signals transmitted by orbiting satellites. It uses the processed information to locate a robot’s velocity and approximate position.

    navigation-positioning-sensor
    Figure 3: Navigation (Positioning) Sensor
  4. Gyroscope sensor

    A gyroscope sensor or Gyro measure uses the angular momentum principle to help maintain orientation. It helps to calculate the rate of revolution in the region of a particular axis. This sensor enables your robot to be independent of the earth's gravity to maintain orientation.

    gyroscope-sensor
    Figure 4: Gyroscope sensor
  5. Sound sensors

    Sound sensors in robotics work similarly to microphones and connect to circuits that evaluate the amplitude of the sounds to a particular threshold value and report the result to the robot. The noise becomes louder with the increase in amplitude. A simple application is a robot programmed to study wildlife. The sensor can detect and follow loud noises and make them data points for wildlife locations. A more complex application for sound sensors is voice recognition, where the robot responds to commands uttered by the user.

    sound-sensor
    Figure 5: Sound sensor
  6. Proximity sensors

    A proximity sensor in robotics can detect (or ‘sense’) a nearby object without physical contact. The transmitter sends electromagnetic radiation to the adjacent sensor, and the receiver receives and then analyses the interruption feedback signal. The amount of light received inside the area can help to determine the presence (or absence) of neighbouring objects. For the robot, the sensors offer a collision avoidance approach.

    Infrared (IR) transceiver: an IR LED directs an IR beam of light at a target area, any light that is reflected from an object within this area is detected creates an electrical signal.

    Ultrasound sensor: These sensors generate high-frequency sound waves, and the recorded echo indicates the presence of an object. Ultrasound sensors can measure distances as well.

    proximity-sensor
    Figure 6: Proximity sensor
  7. Touch sensors

    Touch Sensors (aka contact sensors) are devices that can detect the touch of an object. These are found in small devices such as micro-switches and limit switches. Robots deploy these sensors to avoid obstacles. The sensors indicate whether the robot can reverse, stop, switch on, turn, and so on if it encounters an obstruction.

    touch-sensor
    Figure 7: Touch sensor
  8. Force sensors

    Force sensors calculate the forces necessary in a robot's various functions, such as material management, machine loading and unloading, or material management. This sensor improves the assembly process for troubleshooting. A force-torque sensor provides the robotic arms with the feel of completing an assembly task, and the internal state sensors measure the end effector.

    force-sensor
    Figure 8: Force sensor
  9. Acceleration sensors

    Acceleration sensors measure the acceleration and tilt of the robot. Two types of forces affect an accelerometer.

    Static force: It is the frictional force that exists between two objects. You can measure this gravitational force to determine how much the robot tilts. This parameter helps balance robots. It can also assess whether a robot is on a flat surface or an incline.

    Dynamic force: It is the acceleration needed to move an object. You can find the speed or velocity of the robot by measuring its dynamic force using an accelerometer.

    acceleration-senso
    Figure 9: Acceleration sensor
  10. Temperature sensors

    Temperature sensors measure heat or temperature changes in their surrounding environment. There are various methods used to measure temperature such as using materials that change resistance, or some that generate changes in voltage across a semiconductor junction when heated or cooled.

    Air temperature, immersion temperature, and surface temperature are all applications for temperature sensing.

    temperature-sensor
    Figure 10: Temperature sensor
SharePostPost

Stay informed


Keep up to date on the latest information and exclusive offers!

Subscribe now

Data Protection & Privacy Policy

Thanks for subscribing

Well done! You are now part of an elite group who receive the latest info on products, technologies and applications straight to your inbox.

Technical Resources

Articles, Solution Guides, Webinars, and more.
Keeping you on top of innovations.